4/16/2019 7:45 PM | |
Joined: 3/9/2012 Last visit: 5/22/2024 Posts: 236 Rating: (0) |
Hello, i need the setup for FM350-1 i use operating system Win 10 Thanks |
4/17/2019 8:02 AM | |
Joined: 1/5/2015 Last visit: 2/26/2024 Posts: 108 Rating: (4) |
Hi, Are you using Simatic Manager or Tia portal? |
4/17/2019 11:45 AM | |
Joined: 3/9/2012 Last visit: 5/22/2024 Posts: 236 Rating: (0) |
I use Simatic. |
4/17/2019 12:57 PM | |
Joined: 9/27/2006 Last visit: 6/4/2024 Posts: 12260 Rating: (2670)
|
Hello TheoTheNtal; To work with Windows 10 64 bit, you need Step 7 v5.6 (now with SP1). The Compatibility List provided with the Profduct Note of Step 7 v5.6 SP1 shows the requirements for your FM 350-1 to operate with this version of Step 7: it must be a 6ES7350-1AH03-0AE0 of version 6.0.2 or higher. Service Pack 1 for STEP 7 V5.6 https://support.industry.siemens.com/cs/ww/en/view/109760423 The FM 350-1 configuration package is part of the Step 7 v5.6 software installation, as is described in the documentation for the Step 7 v5.6 SP1: - Folder "FM Configuration Package" Configuration of the function modules FM 350-1, FM 350-2, FM 351, FM 352, FM 352-5, FM 355, FM 355-2, FM 450-1, FM 451, FM 452, FM 455 You can also download for the FM configuration packages for Step 7 v5.6 SP1 here: FM Configuration Package https://support.industry.siemens.com/cs/ww/en/view/60237759 Hope this helps, Dniel Chartier |
Last edited by: dchartier at: 4/17/2019 12:58:53 PMLast edited by: dchartier at: 4/17/2019 1:40:25 PM |
|
This contribution was helpful to3 thankful Users |
4/18/2019 8:17 AM | |
Joined: 1/5/2015 Last visit: 2/26/2024 Posts: 108 Rating: (4) |
Hi, There is also this video in youtube that goes step by step configuration of the example provided by dchartier. Here is the LINK BR |
4/18/2019 11:13 AM | |
Joined: 3/9/2012 Last visit: 5/22/2024 Posts: 236 Rating: (0) |
i have download the setup and i have installed to my operating system it is working!! Thanks!!!! |