10/25/2018 11:11 AM | |
Joined: 10/26/2015 Last visit: 9/23/2024 Posts: 7 Rating:
|
Hello I have a wincc 7.0 system with two redundant servers communicating with a s7 300 controller. Following a power interruption the main server lost the connection with the PLC passing the hand to the secondary server. The next day after another cut on secondary server to his lost the communication with the automaton.to date it is impossible for the two servers to communicate with the plc. can someone help me to solve this problem? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/25/2018 12:02:17 PMNew subject after splitting |
|
Follow us on