9/26/2019 1:44 PM | |
Joined: 5/6/2019 Last visit: 9/18/2024 Posts: 78 Rating: (0) |
Hallo, I was controlling the Sinamics S120 Cu310 2 PN using the PLC S7 1500. I was running the motor to a certian position at different velocity and acceleration. But, many times I am getting the warning or error Following error monitoring window exceeded. The configuration of following error is at 5mm. The screenshot is attached here. The different acceleration that I tried at 250mm/sec is attached in the document. Also finally the trace when error occurs is also attached. My question is how can I avoid the following error? thank you. Attachmentfollowing error.pdf (594 Downloads) |
9/26/2019 4:14 PM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (300) |
Hi, are you online with the drive? You need to be online. |
Best regards, |
|
9/26/2019 4:22 PM | |
Joined: 5/6/2019 Last visit: 9/18/2024 Posts: 78 Rating: (0) |
oh yes, I was offline ;-) |
Follow us on