6/15/2016 4:35 PM | |
Posts: 75 Rating: (19) |
To modify the font use the text format properties of a Symbolic I/O Field (see attachment) |
This contribution was helpful to1 thankful Users |
6/16/2016 1:24 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (194) |
The configured font type in the TIA Portal settings only affect the font in text editors like the VB-Script Editor. What you could do is to add a graphic list and ist elements with no text, then use the export-function. You can open the .xlsx file (in Excel or similar) and use the font you want to use in the runtime to get the alignment right. Afterwards just import the file. ... and in case the displayed font sizes differ between RT and engineering:
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
Follow us on