Industry Online Support
Technical Forum
11/14/2008 12:59 PM | |
Posts: 19 Rating: (1) |
I have now made up two programs that handles counters using Interrupt routines. Just download and try! My example uses an encoder with 1000 pulses/rev, but you can easy change to what ever you have. I have used the example "Tsspeed01" as base for my program. We should all share more of our knowledge with real examples instead of links to a manual that is completly impossible to understand.A proper example with explanations is the best and quickes way to learn. Feedback is welcome. If somebody knows how to start and stop an Interrupt routine and measure the time is was active you are more then welcome with some code. I intend to count low revs of a shaft with a proxamity switch(72 rpm). As too few pulses are generated for a High Speed Counter i have to figure something else out. AttachmentEncoders.zip (310 Downloads) |