2/2/2009 11:00 AM | |
Posts: 16 Rating:
|
Thank you for the advice. Tried, failed... I've defined a message frame extension (drives-messageframe.gif in the attachment), assigned actual force value in it (messframeext.gif) and tried to make it a force sensor (forcesensorconfig.gif, 280 is address of that message frame extension). It didn't work. If this really can be done this way, there are some more questions: 1) What to set as "number of usable bits"? Maximum is 31, but the force value should be LREAL (at least it is displayed with decimal point in expert list - see driveexplist-forceactvalue.gif). 2) What does "format" mean? I get the signed/unsigned thing, but what justification? Is it something with little/big endian? 3) "Min/max raw value" - if the value is real, what to put here? 4) "Min/max technology value" - here I would put the motor's maximum configured force, right? I'm just confused by that the force is already being transmitted from the drive, in correct physical units (N) and the value seems to be OK. So why to create message frame extensions, define virtual force sensors and recalculate the force from bits, raw and technology values, when it should be easy to just take r80 and use it? But how? I'm using Scout 4.1.1.6 and Simotion core of the same version. Attachmentforcecontrol.zip (557 Downloads) |
Last edited by: Mira at: 2/2/2009 11:02 AM |
|
Follow us on