10/14/2014 8:57 PM | |
Posts: 2 Rating:
|
We are trying to upgrade communications of an Windows NT PC-based application that is working since 1999 in a customer plant. The communication between Application/SAPI_S7 and PLC S7315 is supported on Profibus by a CP5613 on the PCstation. We implemented the new configuration on Windows Vista with SIMATIC NET 2008 to preserve the old CP5613 and to operate on a OS still supported (for the moment) using NCM and NETPRO and porting the old parameters in the new environment. I'm not sure about the values to assign to the Local and Remote TSAP. As it can be seen in the attachment, in the Windows NT config the values are 01.00 and 01.00. I'm not able to give the same addresses in the new configuration. I would keep the same values but the proposed min value are respectly 10 and 03. How could I configure it ? Should it be enough, in the current config mode (NCM/NetPro) to set the right values for RACK and SLOT keeping the TSAP computed values ? PS: we are configuring the PC-STATION in lab, hence, during this fase, the PC-Station is not connected to the PLC of the plant Thanks a lot in advance. Augustus
AttachmentCP5613.pdf (72 Downloads) |
Last edited by: Yeanth at: 10/15/2014 9:59 AMLast edited by: Yeanth at: 10/14/2014 9:07 PM |
|
Follow us on