3/22/2017 10:42 AM | |
Joined: 8/3/2009 Last visit: 9/16/2025 Posts: 16412 Rating:
|
Hello You could use industrial Databridge. This you could also use without WinCC. But there are special CPs for some Simatic PLCs that could write direct from PLC into SQL Server Database. Or you use a OPC UA Client and add a SQL ODBC Data connection to write into SQL Server by yourself. A Template you find here: https://support.industry.siemens.com/cs/ww/en/view/109737901 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
3/22/2017 10:56 AM | |
Posts: 29 Rating:
|
Great Murof! To check if I understood what you meant now: 1. I can set up an OPC server 2. Install client on the PC I want to host the SQL Server Database 3. Is "SQL ODBC Data connection" the part I have to code myself?
|
Follow us on