2/9/2022 8:54 PM | |
Posts: 257 Rating: (75)
|
Hello forum community, For all WinCC systems, whether in the TIA Portal or outside of it, there are many options with which the functionality can be flexibly expanded. In the field of process management (PM), there are so-called PM add-ons that are often used in this environment and optimally complement the WinCC product family. Typical requirements that can be solved with these are:
A first overview of the available add-ons is shown in the following FAQ: https://support.industry.siemens.com/cs/ww/en/view/109779954 Further information is available either in the Siemens Industrial Online Support via product notifications of the corresponding add-on or directly from the WinCC Competence Center in Mannheim, which is available for questions and services. This can be reached at: Siemens AG Your sincerelly SIMATIC International Technical Support Hub |