7/7/2013 1:43 PM | |
Posts: 2964 Rating: (481) |
Hello, Try to keep S7 online-->PC com port Uss and check.. Check this link for the informations... http://support.automation.siemens.com/WW/view/en/31657012 Regards, Prakash |
7/7/2013 5:13 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
http://support.automation.siemens.com/WW/view/en/68792063 |
This contribution was helpful to1 thankful Users |
7/7/2013 6:59 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
Ohk.. i was not knowing this... Thanks |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/8/2013 10:07 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating: (31) |
sinamics series controller supports USS type Communications? regards, VP |
Last edited by: viralpatel at: 7/8/2013 10:09 AM |
|
7/8/2013 2:59 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
yes.. check the link given by UMENCHO |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/9/2013 5:25 AM | |
Posts: 664 Rating: (17) |
Hai Ashutosh Kr, Thanks for the valuable reply. The Problem is with Version of software. Thanks&Regards, Raj |
This contribution was helpful to2 thankful Users |
7/27/2013 7:06 AM | |
Posts: 10 Rating: (0) |
I AM USING STARTER VERSION 4.2, I AM FACING SAME PROBLEM.WHICH VERSION I HAVE TO USE.I AM USING CU240B-2 AND CU240E-2 DRIVES.I CANT ABLE TO GO ONLINE. |
Follow us on