Industry Online Support
Technical Forum
9/16/2014 5:38 PM | |
Joined: 8/31/2005 Last visit: 2/11/2025 Posts: 2198 Rating:
|
Yes there are two generations of CUs. Your one is 1st generation. All 2nd generation CUs have a "-2" in the name. A 1st generation CU can only use a FW 3.x. You will have to use a GSDML File (e.g. from http://support.automation.siemens.com/WW/view/en/26641490) to import your drive into TIA Portal. The drive itself is parametrated with STARTER (http://support.automation.siemens.com/WW/view/en/26233208). You will have to enter the communication configuration two times: in STARTER and in TIA Portal. Make shure they are identic. |
|
|
Follow us on