8/26/2023 6:02 PM | |
Joined: 10/4/2019 Last visit: 2/18/2025 Posts: 117 Rating:
|
i have the CU240E-2 PN unit am documenting this PDFConverter with the CU240B-2 and CU240E-2 Control Units (siemens.com) the problem i have is that when some parameters are mentioned like p1070 and p1071 and some other parameters ,i did not find them in Tia portal. even with extended parameters are they accessible only from the BOP !! can you provide me with document which is easy to understand in order to master the G120 programing kind regards |
9/2/2023 9:14 PM | |
Joined: 2/15/2023 Last visit: 2/17/2025 Posts: 4 Rating:
|
Try commision the drive with expert setting. i will reveal more settings. |
Follow us on