1/20/2019 8:33 PM | |
Joined: 11/29/2006 Last visit: 1/29/2025 Posts: 19 Rating:
|
Hi, Sinamics G120 CU250S-2 PN Firmware V4.7 SP10 GSDML TIA V14 I need a file. Best Regards |
1/21/2019 7:50 AM | |
Joined: 10/11/2006 Last visit: 1/22/2025 Posts: 5985 Rating:
|
Hello, ChristophD is right, it seems that the GSDML file will not be sufficient as you seem to have the drive added as a real configuration in TIA Portal and not only as a GSDML file. In this case you will need to use Startdrive V15 with the sufficient HSP. Here you can find all the information and downloads: https://support.industry.siemens.com/cs/ww/en/view/109756820 (the GSDML files are also available for download there, but as said before I think you will need the real integration of the drive) |
With best regards, |
|
Follow us on