1/30/2015 7:14 AM | |
Joined: 3/1/2011 Last visit: 9/3/2024 Posts: 26 Rating:
|
PM250 CU240SPN When Power on AC drive It shows error message as shown in Photographs and we have to do power on and off AC drive frequently at least 10 to 15 time then CU shows Ready signal.There is not fault number showing on BOP just ready led is showing red onCU. At running condition there is not any problem in Ac Drive.It happens only when they switch off drive and on again. what can be the problem? Attachmentfault.zip (150 Downloads) |
Follow us on