7/19/2024 3:41 PM | |
Joined: 6/26/2023 Last visit: 2/1/2025 Posts: 5 Rating:
|
Dear Siemens Support, We have recently added a G120 drive to our existing setup, which includes an MM440 drive. The MM440 drive operates with a frequency setpoint range of 0 to 50 Hz, while the G120 drive operates with an RPM setpoint range of 0 to 1000 RPM. When we attempt to increase or decrease the setpoints simultaneously for both drives, they do not operate correctly due to the difference in their respective units (frequency for MM440 and RPM for G120). Could you please provide guidance on how to properly scale the setpoints to ensure both drives operate in harmony when controlled with the same digital inputs? Additionally, can the G120 drive's setpoint be changed from RPM to frequency to match the MM440 drive? ------------------------------------------------------------------------------------------ |
Last edited by: anil02573 at: 07/20/2024 03:08:37Last edited by: Wit_Moderator at: 07/22/2024 12:19:36New subject after splitting |
|
7/21/2024 9:25 PM | |
Posts: 4 Rating:
|
Find and change the set r0002 = r0024 below |
Follow us on