Industry Online Support
Technical Forum
3/1/2019 6:30 AM | |
Joined: 2/17/2019 Last visit: 10/8/2024 Posts: 1 Rating:
|
hello, I am from India. We have Siemens G120 Drive with details as mention below, SINAMICS CONTROL UNIT CU 240E-2DP Order No. 6SL3244-OBB12-1PA1 SINAMICS POWER MODULE 240 MLFB NO. 6SL3224-OBE21-1UA0 , VER. DO2 We have installed above product in our working site, We are using STARTER Software for its Commissioning.The problems we are facing is as mentioned below, Problem Description- In the Expert list option, The Parameter "P10" i.e Drive Commissioning Parameter Filter only takes " [29] Only Siemens int " instead of [0]Ready Or [1]Quick Commissioning or any other options. We are unable to configure the drive and operate the motor. please help me ...... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/1/2019 12:22:22 PMNew subject after splitting |
|
Follow us on