11/2/2022 12:39 PM | |
Joined: 11/12/2019 Last visit: 12/8/2023 Posts: 14 Rating:
|
It's Bitzer CO2 compressor. |
11/2/2022 2:48 PM | |
Joined: 9/21/2012 Last visit: 12/10/2023 Posts: 3799 Rating:
|
Are both motors connected correctly? The otherone might be connected as DELTA. |
11/3/2022 7:28 AM | |
Joined: 11/12/2019 Last visit: 12/8/2023 Posts: 14 Rating:
|
The motor can only do up to 315 rpm (18%). |
5/3/2023 10:52 AM | |
Joined: 3/27/2008 Last visit: 12/11/2023 Posts: 1042 Rating:
|
Feedback, excellent. |
Tractor |
|
This contribution was helpful to
1 thankful Users |
Follow us on