11/30/2020 8:57 AM | |
Joined: 6/8/2013 Last visit: 12/26/2024 Posts: 158 Rating:
|
Dear Experts, I am using S7-1515-2pn PLC & G120C 1.1Kw Drive for pick & place operation, configured & programming done by using TIA 15.1 & start drive in TIA software. (Motor Data : Power 1.1Kw, RPM 1455, Current 2.55A ) Drive are used to control pick & place Indexer( 4 Position CDS cam Indexer with SEW Motor). The CDS indexer have 2 sensor, 1 is to stop indexer & second one is to check the indexer position. So for each start command to drive rotate indexer by 90deg. Drive is configured over profinet with Telegram-1. I want to rotate indexer at 50hz in 900ms. my cycle will repeat at every 1.3 sec. All above application work perfectly up to 70%(40hz) but above it is is giving fault F07901 Drive: Motor overspeed. In TIA help file given belows remedy Remedy: 1) r1084/r1087 parameter didn't see in start drive? 2) How to activate speed limiting controller? So please help ................ Attachmentsew motor Details.pdf (204 Downloads) |
Last edited by: Ashok Naphade at: 11/30/2020 11:46:41 |
|
Follow us on