7/2/2019 1:42 PM | |
Joined: 8/31/2005 Last visit: 5/21/2024 Posts: 2197 Rating: (326) |
In the control word is a Bit (Bit 11) to reverse the direction. Check this bit is never set. |
|
|
7/2/2019 11:18 PM | |
Posts: 125 Rating: (11) |
p1820 can also be used to reverse the output phase sequence by setting it to 1. This parameter exists as of Firmware V4.7 |
7/3/2019 5:59 AM | |
Joined: 4/10/2016 Last visit: 4/11/2022 Posts: 21 Rating: (0) |
This happened during the work. The PLC's software and Drive parameters never changed !! |
7/4/2019 8:23 AM | |
Joined: 10/11/2006 Last visit: 6/4/2024 Posts: 5856 Rating: (793)
|
Hello, |
With best regards, |
|