11/21/2009 10:53 AM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating:
|
Hi Does it working before ? Is this the first working ? Is this a "machine commissioning" ? |
Karl |
|
11/25/2009 5:34 PM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating:
|
Hi Can you make SPOS ? Do this work ? (Spindel-Positioniering) Please try with G33 or G63 funktion. (Look for this in Manual from Siemens) Do work this ? |
Karl |
|
11/26/2009 1:32 PM | |
Joined: 3/3/2008 Last visit: 3/11/2025 Posts: 333 Rating:
|
hi i think you must be getting a message on the left hand side corner . it should be waiting for first thread cut. if you are getting this alarm check spindle md i.34200=1 &34210=0 even after that if the alarm comes then its the problem with external encoder configuration, try to disable the external encoder my making md 34230=1 . regards ram |
12/3/2009 11:32 AM | |
Posts: 159 Rating:
|
Our VTC uses amotor encoder but due to the transmission the control also uses a BERO proxy on the table for zero degrees. This may be something to check for functionality. Thanks, Craig. |
Last edited by: mecky at: 12/3/2009 11:35 AM |
|
Follow us on