3/9/2016 7:10 PM | |
Posts: 4 Rating:
|
Hello, I have a GE profinet network (controlled by a GE PNC001 controller with some GE PNS001 IO-Devices on the Network. I am new to Siemens and do most of my solutions with GE so please be patient with me :) I have several problems getting this started and I have read every manual and thread available but cannot get anything working. My Siemens Setup : PS 307 5A CPU315-2 PN/DP CP 343-1 ADVANCED "U" CONNECTION BETWEEN CPU AND CP ALL MOUNTED ON A RAIL I want to use the CP343 to read and write information from the cpu memory 1) first thing first - I do not have the SIMATIC_NET_CP library in my Step 7 I have searched for 8! hours on this website to find out nothing useful that can be installed. and I have tried them all I have Step7 V5.5 SP4 and there were no SIMATIC_NET_CP with PNIO_SEND PNIO_RECV available to install on my S7 program. please hemp me find one 2) as I create the PLC setup I chose the CP to be in a profinet network and remove the IO-controller checkmark in Options>PROFINET Tab. are there any other configurations I am missing to configure the CP+CPU as an IO device on my existing network? 3) where do I get a GSD file? there is no option to create one as the CPU does nor have the I-Device option, and in the available manuals this in the Only way it is descried. I have attached some screen shots.(cant hurt) Thank you, Stas K Attachment5.zip (38 Downloads) |
3/9/2016 9:08 PM | |
Posts: 4 Rating:
|
just to remove all doubt, the above installation (simatic_net_cp library s7-v5.4+) does not work on my V5.5 S7 ! |
Follow us on