11/2/2021 4:19 PM | |
Joined: 10/11/2006 Last visit: 1/31/2023 Posts: 5410 Rating:
|
Hello, "Motion_DB" is not a programming language. Please use the LAxixCtrl block for axis commands and use SCL for programming. Downloads"LAxisCtrl" One axis function block for all axis types using DB_ANY https://support.industry.siemens.com/cs/de/en/view/109749348 There is an example project, in this application example. Further info: S7-1500/S7-1500T Motion Control overview Function manual "S7-1500/S7-1500T Motion Control overview" (https://support.industry.siemens.com/cs/ww/en/view/109781848) This documentation describes the general Motion Control functions independent of technology objects. Using S7-1500/S7-1500T axis functions Function manual "S7-1500/S7-1500T Axis functions" (https://support.industry.siemens.com/cs/ww/en/view/109781849) This documentation describes the Motion Control functions for the following technology objects: • Speed axis • Positioning axis • External encoder Using S7-1500/S7-1500T measuring input and output cam functions Function manual "S7-1500/S7-1500T Measuring input and output cam func-tions" (https://support.industry.siemens.com/cs/ww/en/view/109781852) This documentation describes the Motion Control functions for the following technology objects: • Measuring input • Output cam • Cam track Using S7-1500/S7-1500T synchronous operation functions Function manual "S7-1500/S7-1500T Synchronous operation functions" (https://support.industry.siemens.com/cs/ww/en/view/109781851) This documentation describes the Motion Control functions for the following technology objects: • Synchronous axis • Cam (S7-1500T) • Leading axis proxy (S7-1500T) Using S7-1500T kinematics functions Function manual "S7-1500T Kinematics functions" (https://support.industry.siemens.com/cs/ww/en/view/109781850) This documentation describes the Motion Control functions for the following technology objects: • Kinematics (S7-1500T) S7-1500/S7-1500T Motion Control alarms and error IDs Function manual "S7-1500/S7-1500T Motion Control alarms and error IDs" (https://support.industry.siemens.com/cs/ww/en/view/109781853) This documentation describes the technology alarms of the technology objects and the error identifications of the mo-tion control instructions.
|
With best regards, |
|
1/20/2022 10:50 AM | |
Joined: 11/28/2020 Last visit: 2/12/2022 Posts: 4 Rating:
|
*second attachment |
Follow us on