9/21/2011 1:08 PM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Hello, There is not a "pdf printer" driver that can be installed. The idea was to select a "real" network printer which is connected to the PC. http://support.automation.siemens.com/WW/view/en/13336639 Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
9/21/2011 1:15 PM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
No i mean if the pdf-printer is installed at a pc. Take a look at this FAQ: What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)? So you can also print to a printer wich is connected at a pc. Wich printer driver you uses at the pc isn`t interessting for the panel. |
9/22/2011 2:57 AM | |
Joined: 2/28/2011 Last visit: 2/28/2025 Posts: 6 Rating:
|
Hi, |
Follow us on