3/21/2016 1:49 PM | |
Posts: 16 Rating:
|
Thanks a lot...Hope this would help me to spot a similar issue... i would like to find...what exactly would cause this problem... this "Area length error" keeps appearing for me when the program is running fine. will the Processor go to STOP FAULT. if this keeps accumulating. At times it went to STOP FAULT and i predicted a possible cause and fixed it. where im using indirect addressing to a pointer where the program happen to calculate a wrong DBD number at some point. when i open a DB and inside a loop. it caused Stop Fault with Scan time exceed. Now after fixing it, Stop Fault doesnt occur again. But, Area length error keeps coming.. Will the above said method of deleting OB121 will help me to solve the issue. its a machine in production. So, i just wanto be sure before asking for it. Pls suggest. Pls refer to attached Diagnostics Buffer txt. AttachmentDiagnose.txt (406 Downloads) |
Follow us on