4/6/2023 4:07 PM | |
Joined: 1/12/2023 Last visit: 1/4/2024 Posts: 1 Rating: (0) |
If the drive parameters have been adjusted to get the command and speed set point via Profibus then this does require parameter changes. Currently, parameter P554 is set to a value of B3100. I know this has to be changed to something that will tell the drive to get its start command and speed setpoint from Drive Monitor. What does this need to be changed too? Is there anything else that has to be adjusted? It also looks like P368 would have to be something other that a value of 6 which is what I currently have selecting Profibus. ------------------------------------------------------------------------------------------ |
Last edited by: JMcK at: 04/06/2023 17:10:21Last edited by: Jen_Moderator at: 04/09/2023 06:56:37New subject after splitting |
|