12/3/2018 9:18 AM | |
Posts: 21 Rating:
|
There is a problem when I want to download to op7. I used serial cable with correct pinout according to op7 manual and used a RS232/USB convertor for connecting to PC. But when I want download source program to op7 , I have error in the protool. Error E4027 synchronization faulty. No communication to op. RS232 to USB convertor driver is installed too , and I used port COM1 and boudrate 9600 in the protool and device manager (windows). Please help. Why I have error????!!!! thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/3/2018 1:18:15 PMNew subject after splitting |
|
12/3/2018 9:36 AM | |
Joined: 4/24/2006 Last visit: 3/21/2025 Posts: 8904 Rating:
|
Hello, Perhaps this link might help: Why is the connection interrupted while transferring a project with ProTool to an OP? Best regards, Wizard |
12/3/2018 10:16 AM | |
Posts: 21 Rating:
|
OP7 is factory reset. That is empty. Then that show the below message: ”Ready to transfer” I know that’s mean op7 is in download mode. |
12/3/2018 1:50 PM | |
Posts: 21 Rating:
|
Yes. I used COM1 and COM 2. I tested both of them but not working. Best Regards. |
Follow us on