4/8/2022 9:16 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello wreng unfortunately this is not possible in the basic functionality. Have a look at this FAQ: https://support.industry.siemens.com/cs/de/en/view/57132412 .... How do you determine the current mouse position by VBScript?In order to read the current mouse position, you have to access the API (Application Programming Interface) of the operating system. Access to the operating system's API by means of DLLs is not supported in VBScript. .... Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
4/8/2022 10:26 AM | |
Joined: 7/27/2008 Last visit: 11/8/2023 Posts: 25 Rating:
|
hello Murof Thank you so much. best reguard |
Follow us on