9/21/2016 8:01 AM | |
Posts: 11 Rating:
|
Hello, Recently one of our clients ask us to give visibility to our machines on its industrial LAN. We use PLC from siemens but with only one ethernet port, so we cannot provide the plc other address into the industial LAN. The idea is to get some information from the PLCs using an OPC server (Simatic .NET V13) running into a server under the industrial LAN. Our local dealer from siemens sugested us this device but I think it is beyond our requirements. https://support.industry.siemens.com/cs/es/es/pv/6GK5615-0AA00-2AA2/td Do you know how can I make this routing? Thank you in advace. Regards. |
9/21/2016 8:50 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating:
|
Would a router or gateway between the two networks work as well? |
~(‾▿‾)~ |
|
9/21/2016 9:16 AM | |
Posts: 11 Rating:
|
We are using 1512 and 1510 (Format ET200SP) Something like this should work. https://support.industry.siemens.com/cs/attachments/67700710/GH_CP1543-1_76.pdf |
Last edited by: umiguelc at: 9/21/2016 9:29:44 AMLast edited by: Min_Moderator at: 9/21/2016 12:56:02 PMReplace link with permanent one |
|
9/21/2016 9:31 AM | |
Posts: 11 Rating:
|
Our format is ET200S, Siemens told us that there is no CP compatible. |
9/21/2016 11:00 AM | |
Posts: 11 Rating:
|
Thank you all. |
This contribution was helpful to
1 thankful Users |
Follow us on