6/25/2024 7:26 PM | |
Joined: 1/25/2019 Last visit: 11/21/2024 Posts: 2 Rating: (0) |
I would like to graph an array of data where X[i] is the X axis and contains up to 500 data and Y[i] contains up to 500 data forming the pair (X[i],Y[i]) and will refresh them every 100 ms ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/26/2024 09:29:19New subject after splitting |
|
6/25/2024 7:50 PM | |
Joined: 7/25/2017 Last visit: 1/15/2025 Posts: 338 Rating: (54) |
If it is every 100ms, then you might be better off using a custom control that is fed real time tag data. |
Follow us on