3/1/2018 9:45 AM | |
Posts: 2 Rating:
|
Hello everyone, - TIA Version including SP / upd : TIA V14 SP1 Update 1 & WinCC Advanced V14 SP1 Update 1. - Hardware identification : 315/2 PN/DP & TP1200 Comfort - Doubt / problem (keyword) : GRAPH (SFC) display - Application description (scenario) : Can't display it on the HMI. - What type of information you are looking for : Is it possible with an S7-300 ? I'm wondering if there is a way to display a GRAPH (Sequential Function Chart) on my Comfort HMI, knowing that my CPU is a 315-2 PN/DP. It's possible with an S7-1500 (we did it on another project), but when I try to link my S7-300 GRAPH variable to the HMI object, it says that my variable "isn't of the S7Graph type", while the exact same variable seems to be OK on the S7-1500 (see attachments 1 and 2). By the way, the documentation says that we should link "the DB" : on the S7-1500 project, a boolean of that DB (OFF_SQ) was linked without any problem. I'm wondering if it has something to do with the fact that I can't access the variable of my S7-300 from the HMI with "symbolic addressing" while it's possible with that of my S7-1500 (see attachments 3 and 4). Thank you. AttachmentGRAPH on S7-300.zip (44 Downloads) |
3/7/2018 4:10 PM | |
Joined: 8/3/2009 Last visit: 4/23/2025 Posts: 15311 Rating:
|
Hello Aymann What you want to do is clear but unfortunately not possible. The Graph Controls in winCC Comfort/Advanced are part of the Option Prodiag. This Option you can only use with S71500 PLCs in Version V2.X and at least V14. you cannot use Classic PLCs like S7-300/400 and its not the same as ProAgent/PDigag in the Classic world!!! If you need more Information you can read here: https://support.industry.siemens.com/cs/de/en/view/109740151 Bye Murof |
Last edited by: Murof at: 3/7/2018 4:11:10 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
Follow us on