Industry Online Support
Technical Forum
10/11/2021 3:47 PM | |
Joined: 2/10/2020 Last visit: 9/5/2022 Posts: 4 Rating:
|
How do you do this inside a faceplate? From what I can see it is only possible to use external text and graphic lists which makes it extremely difficult to configure the faceplates correctly. Even when choosing a graphic list in the resource list option when using the faceplate in a window, the graphic is not shown, and the panel has to be simulated in order to see the graphics. It appears as an invisible object in the faceplate editor, and makes it very hard to align the graphic to where I want it placed, and allign statussymbols on top of the graphic list. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2021 08:07:13New subject after splitting |
|
Follow us on