2/14/2022 8:50 AM | |
Joined: 11/23/2015 Last visit: 9/10/2024 Posts: 33 Rating:
|
Hello, I am suffering from the same issue with WinCC 7.5 SP2 Upd5. The graphics runtime freezes and the computers (OS Server & OS Client) became inoperative. Most of the times, when ONLY restarting the graphics runtime (not stopping the runtime at all) is dealing with the problem. So far we have installed the latest update of the version Update 7 and now we are observing the behavior of the system. When the graphics runtime freezes the Pdlrt.exe is using approx. 1.2 GB memory and when I restart the exe it starts from 50-60 MB. Have you came up with some other solutions to the problem or it is most commonly an update matter of the system? Best Regards, Alex ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/14/2022 13:02:20New subject after splitting |
|
2/15/2022 1:44 PM | |
Joined: 2/17/2020 Last visit: 9/12/2024 Posts: 1057 Rating:
|
Hi again, Ok, they are released, but it would be useful to take into account the note of this FAQ with the OS Client (20H2): "Notes on current updates: "20H2" and SQL server Subsequent to the installation of the Windows 10 October 2020 update ("20H2"), there may occur problems with the SQL server installation. As a consequence, the WinCC basic installation is disturbed as well. Cause for the error is an outdated version of the Microsoft Edge browser. Install the current version (v86.0.622.56+ or higher) to correct the error. To this end, open the "..." menu in Edge and select the menu entry "Help and feedback -> About Microsoft Edge". This will automatically start the update process. Afterwards, perform a restart.". |
A rating will be well appreciated. |
|
2/16/2022 8:40 AM | |
Joined: 4/28/2015 Last visit: 4/11/2024 Posts: 8 Rating:
|
I think we have the same problem
|
2/16/2022 8:41 AM | |
Joined: 4/28/2015 Last visit: 4/11/2024 Posts: 8 Rating:
|
|
2/16/2022 8:48 AM | |
Joined: 4/28/2015 Last visit: 4/11/2024 Posts: 8 Rating:
|
The operating system version of the OS client is also 20h2 |
2/16/2022 8:48 AM | |
Joined: 4/28/2015 Last visit: 4/11/2024 Posts: 8 Rating:
|
|
2/16/2022 8:49 AM | |
Joined: 4/28/2015 Last visit: 4/11/2024 Posts: 8 Rating:
|
|
Follow us on