Industry Online Support
Technical Forum
12/12/2007 4:47 AM | |
Joined: 9/27/2006 Last visit: 12/1/2023 Posts: 12183 Rating:
|
Hello New_bird; Here is a link to the Simatic CPUs gsd files, you can locate your CPU in the list and dowload the specific gsd file, or dowload them all at once if you need them: http://support.automation.siemens.com/WW/view/en/113652 What exactly is your project requirement? Are you using a non-S7 Master and the CPU341-2C DP as a slave? If you are using a Siemens S7 master, you should have the gsd already included in HW Config; there are FAQs on the Product Support section (see the above menu) that will show you the exact steps to configurea DP master/slaveconnection between 2 S7 CPUs. Hope this helps, Daniel Chartier |
12/12/2007 6:32 AM | |
Posts: 17 Rating:
|
Dear Dchartier, Thanks for the reply. I got it after I installed the Simatic S7v5.4 SP3. Anyway, thanks for provided a very useful link. Thank you regards, |
Follow us on