10/14/2017 4:12 PM | |
Joined: 9/27/2006 Last visit: 6/8/2023 Posts: 12037 Rating:
|
Hello Franky; It seems that the IME NEMO 96 uses an add-on module for Profibus communications; the IF96007A is used for the NEMO MD powermeters. Here is the link to the gsd file download for the IF896007A, and a manual that contains references on using the NEMO 96 with a S7-315-2DP Profibus master: http://www.imets.it/sito/details.php?lang=en&id=11&type=f&con=123220062012on http://www.imeitaly.com/protocolli/PR136.pdf Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/14/2017 4:14:29 PM |
|
10/16/2017 2:05 PM | |
Joined: 9/27/2006 Last visit: 6/8/2023 Posts: 12037 Rating:
|
Hello Franky; The status of the IFC4R is "Discontinued", which is probably why it is difficult to locte the protocol files. See the following link: http://www.imeitaly.com/eng/tech_doc.asp?Famiglia=Interfaces&CodiceNT=&CodiceArticolo=&Invio=Invio The technical documents that you can download mention the gsd file but do not show a gsd file name or a download link. So you will have to obtain the gsd file from IME directly. Hope this helps, Daniel Chartier |
Follow us on