11/6/2018 5:07 PM | |
Joined: 9/27/2006 Last visit: 3/27/2025 Posts: 12344 Rating:
|
Hello ahi; Could you explain what exactly your situation is, and what you want to do with this file? A GSD file contains information for a Profibus-DP master (or Profinet IO controller) to integrate a Profibus slave or Profinet IO device in its configuration. As such, the ET 200S module you show would be part the ET 200S IM 151-1 interface module, for example, which you can find here: https://support.industry.siemens.com/cs/ww/en/view/652154 However that file is only useful to integrate the ET 200S in the configuration of a 3rd-party Profibus master. For a S7 CPU, it should already be part of the Profibus catalog of Step 7 (Classic or TIA Portal). For some reason, I do not believe that you are really in need of a GSD file. Again, please explain you situation more clearly. Hope this helps, |
11/6/2018 6:56 PM | |
Joined: 9/21/2012 Last visit: 3/28/2025 Posts: 4348 Rating:
|
Are you perhaps using TIA Portal? TIA Portal doesn't support all old hardware. |
11/7/2018 9:11 AM | |
Joined: 10/23/2015 Last visit: 3/2/2025 Posts: 167 Rating:
|
Hello, Yes i use TIA V14, i think that is right.... Thank you |
This contribution was helpful to
1 thankful Users |
Follow us on