5/17/2019 9:53 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hi, I am looking to a pyronix gsm dialler https://www.pyronix.com/downloads/v2-gsm-user-guide-english-rins1322-8 to tie in with the attached program, so that when Input 4 is triggered this will give a output to the dialler and send the appropriate message to the stored numbers.The small problem I am having is that I only want the output to be active during the machine running hours of 06:00-00:30, because at the moment ever time the machine stops for routine maintenance and cleaning the logged numbers are called to inform them that the machine has stopped.You can guess this has gone down rather well ...but they should be careful what they wish for!!. so before I get hunted down and publicly executed is there a way around this life threatening problem using the LOGO, I cant see anything in the pdf for the dialler that relates to this problem Ade AttachmentACM_LINE2_05_05_2019.zip (125 Downloads) |
5/17/2019 10:06 AM | |
Joined: 12/18/2014 Last visit: 5/20/2024 Posts: 33062 Rating: (4083)
|
Do you mean the output Q1? |
5/17/2019 10:12 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hi, Yes sorry about that |
5/17/2019 10:15 AM | |
Joined: 12/18/2014 Last visit: 5/20/2024 Posts: 33062 Rating: (4083)
|
Should Q1 be switched on constantly, so I4 HIGH signal has? Or should only a temporary impulse be spent? |
5/17/2019 10:29 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
once I4 is energised Q1 is on constantly |
5/17/2019 10:32 AM | |
Joined: 12/18/2014 Last visit: 5/20/2024 Posts: 33062 Rating: (4083)
|
Like this?
AttachmentACM_LINE2_05_05_2019_V2.zip (134 Downloads) |
5/17/2019 10:57 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Just perfect....thank you |
This contribution was helpful to1 thankful Users |