Industry Online Support
Technical Forum
8/27/2014 7:46 AM | |
Posts: 24 Rating: (0) |
Hi experts, Currently I've procured the following hardware (attached in pdf) and would like someone to confirm if either configuration are correct. I am very new to Sinamics therefore need some guidance. Thank you. AttachmentCLIQ and DC Link Config.pdf (121 Downloads) |
8/27/2014 8:00 AM | |
Joined: 5/12/2006 Last visit: 10/2/2024 Posts: 22388 Rating: (3016)
|
Hi, this config ist not possible. The Smart Line can only connect to one Control Unit not to two. Regards Christoph |
8/27/2014 11:24 AM | |
Posts: 24 Rating: (0) |
Do we need to connect the control unit to the smart line module? Or we can just have the smart line module to connect the motor power modules only? |
Follow us on