7/14/2014 10:53 PM | |
Joined: 12/1/2009 Last visit: 2/9/2025 Posts: 672 Rating:
|
Dear PCS 7,
The hardware dongle is a memory moduleplugged into the back of the CP341. Siemens offers additional protocols "loadable drivers"such as Modbus RTU Master which needto be transferred via the HW-Config ontothat dongle.Sowhen you order aloadable driver you will get that dongle with it.
You can use/re-use thatdonglein any other CP341 but the driver will run on the CP withthe hardware dongle installed only.
Yes, you can write your ownsoftware driver or use mine. WITHOUT ANY DONGLE AND TOTALLY FREE OF CHARGE! Download link: Best Regards. |
Give us your feedback and show us your respect! |
|
7/16/2014 5:40 PM | |
Joined: 12/1/2009 Last visit: 2/9/2025 Posts: 672 Rating:
|
Dear PCS 7, I think this is what you are looking for: Best Regards. |
Give us your feedback and show us your respect! |
|
Follow us on