9/5/2015 5:53 PM | |
Joined: 3/28/2015 Last visit: 1/10/2025 Posts: 722 Rating: (214) |
Hello, Kindly check the following: 1-Wiring into analog module. 2-Cables. 3- HW setting. 4- Ground terminal. 5-Test with another module or PT100. 6- Programming if it is a new design. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
9/5/2015 10:46 PM | |
Joined: 3/28/2015 Last visit: 1/10/2025 Posts: 722 Rating: (214) |
Kindly find the attached file. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
6/28/2024 7:16 AM | |
Posts: 1 Rating: (0) |
Dear Sir/Madam, 6ES7331-1KF02-0AB0 module which we procured earlier for emergency situations. The make and model of the received modules are as per our requirements, and these modules were kept in store. Recently, we come across an issue with our existing module. Upon replacing it with the new cards, abnormal temperature parameters arose almost 10 degrees difference (higher) which show the abnormal behavior of module. Pictures are Attached for reference Please inform us why there is temperature difference . Looking forward to your kind response. Best Regards, Khaliq Dad __________________________________________________ [snip] Note: This e-mail and any attachments are confidential and may be privileged. If you are not a named recipient, please notify the sender immediately and do not disclose the contents to another person, use it for any purpose or store or copy the information in any medium.We thank you in advance. |
Last edited by: The Helping Hand at: 06/28/2024 11:53:09Contact data removed, doesn't comply with forum terms. |
|
11/12/2024 10:24 AM | |
Joined: 7/16/2019 Last visit: 1/14/2025 Posts: 1 Rating: (0) |
Merhaba konu çözüldümü acaba ? Nasıl bir yol izlediniz ? |
Follow us on