11/30/2016 9:03 AM | |
Joined: 5/20/2015 Last visit: 9/1/2024 Posts: 34 Rating: (15) |
Hi rajesharihant, Siemens analog modules are very flexible in HART compatibility. Recently i come across with HART level transmitter connection to an ordinary analog input module. And it was successful. Connected Info: TX+ connect to + 24DC, TX- connect to +AI and –AI connect to -24VDC Am also attaching specific Siemens HART modules info with this message. AttachmentHart_analog_modules_manual_en-US_en-US.pdf (382 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on