9/15/2010 6:24 PM | |
Posts: 21 Rating:
|
Hi, The script is good for WinCC flexible RunTime on PC, but unfortunately not on the Panels like MP277,MP377,... which are based on WinCE. Error Code "424 - Object required" is the answer for the PC-script on a WinCE-Panel On WinCE there are a few different things on scripting especially with "file-commands". Has anybody a solution for WinCE-Panels, for a file open-dialog or read the files (optionally the directorys) into variables (or into a text-file) so maybe I can show them in a symbolik IO-field to choose a file ? Hope to findan solution too .... Thanks Splitted from I need to open a file requester from a script in Flexible 2008.... |
Last edited by: O_Moderator at: 9/16/2010 9:00 AMnew subject after splitting Last edited by: woisi at: 9/15/2010 6:37 PM |
|
9/22/2010 11:39 AM | |
Joined: 4/24/2006 Last visit: 9/14/2023 Posts: 8592 Rating:
|
Dear woisi, Perhaps this link might help: how on a Windows-based panel can you use a script to save and read out information in a text file? Best regards, Wizard |
Follow us on