Industry Online Support
Technical Forum
11/11/2011 3:16 PM | ||
Joined: 5/28/2008 Last visit: 5/23/2024 Posts: 1343 Rating: (141)
|
Apart from the CommandTable you should upgrade to SP1 Upd2 and later also to SP2 (if it is released). Don't care about the size. It is as big as the standard installation. Maybe 1-2MB bigger, but not additional 3GB to your standard. With CommandTable you can drive specified profiles. The handling is very easy. Hopefully soon will be an update of CE-X7 available, which shows the functionality of CommandTable
regards |
|