11/24/2016 6:04 PM | |
Posts: 9 Rating:
|
Hi, I am currently dealing with a project which is based on communicating S7-1200 1214C DC/DC/DC PLC with PC(Windows 10) via ethernet. The goal of the project is creating a C# based Windows desktop application. I did some research and ended up using S7.Net for this purpose. I have TIA Portal V13. I have attached a .doc file. I am basically doing the same stuff in the link included in the .doc file. But I keep getting an error saying "InvalidCastException was unhandled" even though I am (supposedly) doing the exact same stuff in the video provided in the .doc file. I guess there is something I am missing. Thanks in advance. Aydin Ozcan AttachmentbitirmeSorun.docx (78 Downloads) |
Follow us on