8/4/2009 11:41 AM | |
Posts: 54 Rating: (0) |
Hi, I tried, but it is still not collect data from 126, pls see my project and give me some advises. TuanNA. AttachmentNewhw2.zip (932 Downloads) |
8/5/2009 11:45 AM | |
Posts: 54 Rating: (0) |
Hi YngSoul, I see all data from PAC3200 canberead, some of them isRead/Write datatype and I see in the table of data, it exist following the register in continous with step is 2. You can see in the data table of PAC3200 attachment with this thread. I think when SIEMENS make PAC3200 with Modbus TCP and point all data in table, that mean it can run with full function of Modbus protocol like connection with CP343-1 and Open Modbus TCP, but the problem is we must read data by step 125 register in each order telegram while we don't have much of trouble shooting guide for it. I am still waiting for... Hope to hear from you soonest, TuanNA. AttachmentOutput1.pdf (876 Downloads) |
Follow us on