1/19/2016 5:00 AM | |
Posts: 3 Rating: (0) |
hi, we need the help for profibus signal mapping of DCM master. I have selected 10word in/10 word put profile. We are configured the following GSD file in our system. GSD - SI04816A.GSI Profile - 10 Word In/10 Word Out (Telegram 220)
We need the following signals from DCM drive over profibus. DI -
1] Drive running feedback 3] Reverse running feedback
DO - 1] Forward start command 2] Reverse start command 3] Quick Stop command 4] Ramp up command 5] Ramp down command
AO 1] Acceleration Rate 2] Deceleration Rate Also We need the details of "Fault Code" and "Alarm Code" list along with code details of drive fault. Please help me to who I will get the above data from drive. Regards, Paigambar Mujawar
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/19/2016 1:02:51 PMNew subject after splitting |
|
Follow us on