Industry Online Support
Technical Forum
11/23/2012 5:41 PM | |||||
Joined: 9/27/2006 Last visit: 9/14/2024 Posts: 12282 Rating: (2683)
|
Hello desmul; The capacity of a S7-317-xxxx or S7-319-xxxx to handle all these I/Os and the amount of programming required should be enough, even though the project looks imposing. See their technical specs in the following links:
As far as the amount of distributed racks (either Profibus-DP or Profinet) you would require for the DO modules, this would depend a lot on the number and type of signals you can implement in a single DO module. For example Siemens offers 64-DO and 32-DO modules, 24 V DC; see the following attachment, taken from the S7-300 Module Data manual. SIMATIC S7-300 S7-300 Automation System Module Data You have to determine what kind of signal your equipment will respond to, if you require intermediate relays... But let's assume for nowthat 64-DO modules are acceptable; your 2000 DOs could be controlled with 32 DO cards. ET 200M interfaces (IM 153-2HF for DP, IM 153-4 for Profinet) support 12 IO modules on ther rack, so you would need 3 distributed racks to connect the controller toyour equipment. By the same calculation, 32-DO modules would need 6 racks, 16-DO modules... Most of these configurations could be setup in a single (double door) control panel. Profibus-DP for example can support up to 125 nodes on the bus, so really that would not be a problem. For your own benefits, I suggest your start out with the S7 controller configurator offered by Siemens in the Siemens Industry Mall. It would be at least a starting point for your project design; https://eb.automation.siemens.com/goos/catalog/Pages/ProductData.aspx?language=en&nodeid=5000008&tree=CatalogTree®ionUrl=/#topAnch Hope this helps, Daniel Chartier |
||||
Last edited by: dchartier at: 11/23/2012 6:47 PM |
|||||
This contribution was helpful to1 thankful Users |
11/25/2012 12:53 PM | |
Posts: 378 Rating: (73) |
Hello dchartier, I never get such a clear and excellent answers Thank you so much you have done a part of my project! Once again Thank you! |
Follow us on