5/8/2012 9:15 AM | |
Posts: 557 Rating:
|
Hello, You can use cpu inbuilt profinet port & have profinet s7 connection in netpro & exchange data with out any problem. |
5/8/2012 9:37 AM | |
Posts: 8946 Rating:
|
Look also or "FDL communication". Point to Point via Profibus. Easy to do. |
This contribution was helpful to
1 thankful Users |
5/8/2012 9:41 AM | |
Posts: 272 Rating:
|
If you are using TIA Step 7 V11then there is one more option. You can also use TCP Client Server on the same PN Network. |
5/8/2012 9:52 AM | |
Posts: 557 Rating:
|
hello, I think you can take saperate cp or PN-PN Coupler for communication. PN-PN coupler work same as dp-dp coupler. |
Follow us on