7/24/2019 3:09 PM | |
Posts: 41 Rating: (0) |
Yes, I understand the problem you are talking about For example, I am not near iot2000 to connect to wifi or connect hardware, I want to login to node red so can it work? |
7/24/2019 4:14 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Yes, if your IOT2000 is in the same network. Kind regards |
7/24/2019 4:55 PM | |
Posts: 41 Rating: (0) |
Can you tell me more clearly, I don't understand |
7/29/2019 8:52 AM | |
Posts: 41 Rating: (0) |
Can you help me with this problem? For example, I'm not near the iot2000 to connect to wifi or connect hardware, I want to log in to the red button so it can work? |
12/31/2021 4:24 AM |
|
Joined: 12/26/2021 Last visit: 12/31/2021 Posts: 1 Rating: (0) |
truyen |