6/9/2011 2:07 AM | |
Joined: 10/7/2005 Last visit: 3/20/2025 Posts: 3042 Rating:
|
Hello Marciano the 443-1EX20 has an2 port switch in it (it isNOT a Hub) andI fearwill only sendoutthe ISO-on-TCPUnicast message via the port to which the partner stationis connected/reachable. You will need to either connect your Wireshark Laptop somewhere into that chain (e.g. via a hub or netwrok tab or switch with montioring port etc)or install Wireshark on the Partner PC and below is linkwhich shows all the options available to you: Wireshark Ethernet Capture setup I hope this helps |
Cheers |
|
This contribution was helpful to
2 thankful Users |
6/9/2011 1:37 PM | |
Posts: 3 Rating:
|
If the CP Port2 is a switch, than make sense not seeing my messages, I will look for the option you have mentioned Thanks |
6/9/2011 9:45 PM | |
Joined: 5/24/2007 Last visit: 4/24/2024 Posts: 284 Rating:
|
That´s good.... Marciano or Mar-us1.. Happy Sniffing Krish |
Follow us on