Industry Online Support
Technical Forum
2/10/2020 2:05 PM | |
Posts: 1 Rating:
|
Hi Experts! I have a problem to read the line speed with a encoder. The HW config is a "profibus equidistante:DP"/ “Isocrono mode” with a count module 24V C V2.0 "6ES7 138-4DA04-0AB0C" on a "ET200S". The count is right but sometime the signal begin to oscillate and the speed calculation fails. I have changed the pfb wire; encoder, counting module; all the connectors ... BUT, THE SAME The speed calculation is executed on an OB35 (50 ms) More information: CPU: 416-2 DP Encoder: GI355 A70C335 BAUMER 5000 RPM. Count: 6ES7 138-4DA04-0AB0C Please help me with the problem . thanks. AttachmentConsulta_encoder.docx (30 Downloads) |
Follow us on